Edmund Optics®使用自己的和第三方Cookie來優化我們網站的技術服務功能。了解我們如何使用Cookie。

  • 我的帳戶
  • 0

Mounted Infrared (IR) Filters

Mounted Infrared (IR) Filters

  • Pass Only Visible Light or Only IR
  • IR-Cut are Ideal for Use As Heat-Absorbing Filters

IR-Cut filters are frequently used as heat-absorbing filters since they let the visible spectral range pass while the infrared rays from 780nm on are strongly blocked. These infrared filters are often used to protect IR-sensitive sensors or used in illumination systems. Note that for intense radiation from UV sources with wavelengths below 320nm (i.e., Xenon lamps), the transmission characteristics can be permanently changed. UV/IR-Cut is a multi-coated interference filter that completely blocks unwanted UV and IR radiation. It is especially recommended for applications where digital image sensors have not been fitted with an IR protection filter (or it was removed). There is little effect on off-axis angles; it is not recommended, however, for extreme angles of incidence. UV/VIS-Cut filters absorb most of the ultraviolet and visible region and transmit the infrared region. For infrared images that consist of a combination of visible and infrared light, we recommend the R-72 Infrared filter (which passes 720nm and above). Note that lenses are typically designed for the visible spectrum, so focusing adjustment is required to obtain clear images in the infrared.


LOADING PRODUCTS...
出口明細

Need a Quote?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Google+ Edmund Optics Instagram

SSL, SSL Certificates, Secure Sockets Layer