Beam Displacement, s (mm) : --
Displacement of Secondary Reflection, x (mm): --
$$ s = t \cdot \sin{\theta} \left( 1 - \frac{\cos{\theta}}{\sqrt{n^2 - \sin^2{\theta}}} \right) $$ |
$$ x = \frac{t \cdot \sin{\left( 2 \theta \right)}}{\sqrt{n^2 - \sin^2{\theta}}} $$ |
s | Beam Displacement |
x | Displacement of secondary reflection |
θ | Angle of incidence between beam and plate normal |
t | Thickness of plate |
n | Refractive index of medium |
Note: This calculator is valid within the following limits: t > 0mm, 0° < θ < 90°, n > 0
Determine the displacement of a collimated beam incident on a tilted plane-parallel plate, or window. This displacement is dependent on the angle of incidence, the thickness of the plate, and the refractive index of the plate. This calculator also determines the displacement of the secondary reflection resulting from a small portion of the beam reflecting off the glass-air interface of the plate.
The exit beam will be parallel to the input beam and magnification remains constant when imaging through a plane-parallel plate.
Question: What is the displacement of a beam and its secondary reflection when the beam passes through a 10mm thick N-BK7 plate at an angle of incidence of 15 degrees?
Answer: The beam displacement and secondary reflection displacement can be determined by:
The displacement of the beam is 0.916mm and the displacement of the beam’s secondary reflection is 3.499mm.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information