Edmund Optics®

知識中心

 由我們 240 多位全球工程師創建且經過驗證的可信任技術資源庫。

Filter
知識中心 資源 (42)

Athermalization Ruggedization

Athermalization is a type of ruggedization that mitigates the harmful effects of thermal expansion and defocus in optical and imaging systems.

現在查看 添加內容至保存

Schwarz Mirrors

Schwarz Mirrors eliminate stray light using black, engineered fused silica substrates that maintain desired characteristics while absorbing unwanted light.

現在查看 添加內容至保存

Ultraviolet Lasers

A new generation of small, cost-effective, CW ultraviolet (UV) lasers allows more applications to move to UV wavelengths for increased power and precision.

現在查看 添加內容至保存

Imaging Systems on the Perseverance Mars Rover

23 unique imaging systems help the Perseverance Mars rover look for signs of water and ancient life on the red planet.

現在查看 添加內容至保存

盡可能減少超快系統的熱透鏡效應

Specialized coatings can minimize thermal lensing in ultrafast laser systems, which are particularly susceptible to detrimental thermal effects.

現在查看 添加內容至保存

桿式反射鏡

Mounting flat mirrors by their edges in a kinematic mount imparts stress onto the mirror surface. This results in distortion and reduced quality of the reflected wavefront, which is especially noticeable when using high-quality mirrors. Stemmed mirrors, on the other hand, are mounted from a smaller diameter “stem” protruding from the back of the mirror, resulting in significantly reduced stress on the mirror surface, high stability, and cost reduction and can be used as a replacement for a more expensive and complex kinematic mount and a conventional mirror.

現在查看 添加內容至保存

Superpolished Optics

Superpolished optics with sub-angstrom surface roughness are ideal for precise laser optics applications

現在查看 添加內容至保存

Single-Material Aspheric Achromats

Single-Material Aspheric Achromats correct chromatic aberrations with a unique geometry, leading to numerous benefits over conventional achromatic lenses.

現在查看 添加內容至保存

大視場遠心鏡頭

Large field of view telecentric imaging lenses allow for reduction of measurement and inspection time. Learn more about large FOV lenses at Edmund Optics.

現在查看 添加內容至保存

超薄高通及低通濾光片

Innovative ultra-thin filters provide flexibility, scratch resistance, and durability comparable to most hard oxide coatings. Learn more at Edmund Optics.

現在查看 添加內容至保存

半導體超級反射鏡

Semiconductor supermirrors offer high reflectivity and outperform many IR mirrors on the market. Learn more about these new supermirrors at Edmund Optics.

現在查看 添加內容至保存

CNC Glass Machining

Computer Numerical Control (CNC) machines used for complex geometry manufacturing are expanding their material capabilities. Learn more at Edmund Optics.

現在查看 添加內容至保存

加固成像鏡頭

Not all ruggedized imaging lenses feature the same type of ruggedization. Learn about the advantages and disadvantages of each type at Edmund Optics.

現在查看 添加內容至保存

Open-Source DIY Microscopy

Accessible, Flexible Technology Supported by a Community of Users

現在查看 添加內容至保存

Integration with Consumer Electronics

Bringing Professional-Grade Technology to All

現在查看 添加內容至保存

快速建立光學產品原型

Quickly Respond to Collapsing Product Lifecycles

現在查看 添加內容至保存

未來的顯微鏡物鏡

Advances in Microscopy Tackle the Challenges of the Future

現在查看 添加內容至保存

Computer Generated Hologram Metrology

Computer Generated Hologram metrology provides a new solution for overcoming traditional asphere metrology. Learn more about CGH metrology at Edmund Optics.

現在查看 添加內容至保存

光學濾光片的未來

New optical filters are being developed due to the advancements in applications and technologies. Learn more about the future of filters at Edmund Optics.

現在查看 添加內容至保存

Additive Manufacturing

Additive manufacturing is revolutionizing rapid prototyping, IP protection, and the job market in the optics industry

現在查看 添加內容至保存

全面採用非球面透鏡

Time to Replace Spherical Elements with Aspheric Lenses

現在查看 添加內容至保存

2018 年的四大趨勢

Advances in microscopy, imaging, and extreme ultraviolet optics

現在查看 添加內容至保存

Top 4 trends 2019

Advances in Smart Materials, Imaging, and Ultrafast Laser Optics

現在查看 添加內容至保存

高反射率反射鏡適合雷射應用

The industry standard method for quantifying reflectivity does not tell the whole story

現在查看 添加內容至保存

非直視性成像

Seeing around corners is no longer science fiction thanks to ultrafast lasers and sensitive cameras

現在查看 添加內容至保存

系統微型化適用的非圓形光學元件

Trimming the Fat: Truncating Lenses to Shrink Systems

現在查看 添加內容至保存

Reflective Laser Beam Shaping

Beam Shaping for High Power and Short Pulse Durations

現在查看 添加內容至保存

Hyperspectral and Multispectral Imaging

Hyperspectral imaging (HSI) and multispectral imaging (MSI) are two related technologies that make use of specialized vision systems to acquire extra image information from extended regions of the electromagnetic spectrum aside from the visible spectrum.

現在查看 添加內容至保存

Ruggedized Imaging Systems for Harsh Environments

The growth of automation has introduced machine vision lenses to more harsh environments involving shock, vibration, contaminants, and temperature swings.

現在查看 添加內容至保存

Free-Space Optical Communication

Free-space optical (FSO) communications wirelessly transmit data through the air using lasers. FSO promises to revolutionize broadband internet access.

現在查看 添加內容至保存
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin