Edmund Optics stocks a comprehensive selection of Acktar®’s ultra-black light-absorbing products, engineered for advanced optical systems that demand maximum stray light control. Featuring proprietary coatings like Metal Velvet™ and Spectral Black™, Acktar’s foils and components offer total hemispherical reflectance as low as ~1% across the visible (VIS), short-wave infrared (SWIR), and long-wave infrared (LWIR) ranges.
Unlike traditional black paints or carbon nanotube coatings, Acktar® products are dry, non-particulate, cleanroom and vacuum compatible, with no outgassing or curing. Their peel-and-stick application supports easy integration onto curved, irregular, or compact surfaces.
Edmund Optics offers an extensive range of Acktar® light-absorbing products off the shelf, including foils, films, panels, laser beam traps, pinholes, air slits, and C-Mount noise-reduction tubes—ideal for imaging, IR, and laser systems. Sizes range from 1" die-cuts to 50-meter rolls, offering unmatched flexibility for both prototyping and production.
With the industry’s widest selection of off-the-shelf Acktar® foils, off-the-shelf availability, and global fulfilment, Edmund Optics provides a convenient one-stop shop for blackening products and beyond.
About Edmund Optics®:
With over 80 years of experience, Edmund Optics is a trusted provider of high-quality optical components and solutions, serving industries like Life Sciences, Biomedical, Industrial Inspection, Semiconductor, and R&D. The company employs 1,300+ people across 19 global locations and continues to grow.
As a leading optics and photonics company, Edmund Optics provides two specialized solutions: a robust Marketplace with 34,000+ off-the-shelf products and Advanced Manufacturing, which focuses on custom and volume production of precision optical and imaging components.
Edmund Optics’ Marketplace is a one-stop shop for over 34,000 in-stock products from in-house manufacturing and 40+ top-tier brands, covering the entire beam path with fast, easy purchasing. For tailored solutions, Advanced Manufacturing offers custom design, first-article production, and scalable manufacturing — supported by four global design centres and nine specialized factories producing over 2 million components and 175,000+ assemblies annually.
Learn more at www.edmundoptics.com
Contact:
Agnes Huebscher, Senior Director, Global Corporate Marketing and Communications
[email protected]
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
Privacy Policy | Cookie Policy | Terms & Conditions | Accessibility
California Consumer Privacy Act (CCPA): Do Not Sell My Information
The FUTURE Depends On Optics®