eo_logo
 
Product added to cart

Edmund Optics Expands In-Stock Offering to Include Single-Mode Patchcords

FC/PC & FC/APC configurations now readily available for fast procurement

11/24/2025, Barrington, NJ USA   —

Edmund Optics, a leading global provider of optical and imaging technology solutions, has expanded its in-stock offering with the addition of Single Mode Fiber Optic Patchcords, available in stock and ready to ship. The range provides customers with a fast-sourcing option for patchcords ideal for beam delivery, sensing, microscopy, and telecom applications.

Available in FC/PC and FC/APC connector types and in 1 m, 2 m, and 5 m lengths, the patchcords cover wavelengths from 450–1650 nm. Each assembly features clearly engraved connectors for quick identification and smooth integration into existing setups.

By keeping multiple Single Mode Fiber Optic Patchcord configurations in stock, Edmund Optics ensures customers can quickly source the parts required for their applications. When paired with the company’s 34,000+ component portfolio, this makes it easier for labs, integrators, and OEMs to maintain project momentum.

 

About Edmund Optics

With over 80 years of experience, Edmund Optics® is a trusted provider of high-quality optical components and solutions, serving industries like Life Sciences, Biomedical, Industrial Inspection, Semiconductor, and R&D. The company employs 1,300+ people across 19 global locations and continues to grow.

As a leading optics and photonics company, Edmund Optics provides two specialized solutions: a robust Marketplace with 34,000+ off-the-shelf products and Advanced Manufacturing, which focuses on custom and volume production of precision optical and imaging components.

Edmund Optics’ Marketplace is a one-stop shop for over 34,000 in-stock products from in-house manufacturing and 40+ top-tier brands, covering the entire beam path with fast, easy purchasing. For tailored solutions, Advanced Manufacturing offers custom design, first-article production, and scalable manufacturing — supported by four global design centers and nine specialized factories producing over 2 million components and 175,000+ assemblies annually. Learn more at www.edmundoptics.com.

 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin
;