Edmund Optics® (EO), the premier provider of optical components, introduces its new TECHSPEC® BBAR Coated Hypotenuse Right Angle Prisms. These broadband anti-reflection (BBAR) prisms feature a wide wavelength range from 350 - 2200nm and are ideal for applications that require a single axis retroreflector and optical systems with space limitations.
Angle tolerance of ±15 arcsec
TECHSPEC® BBAR Coated Hypotenuse Right Angle Prisms provide a tight angle tolerance of ±15 arcsec, reducing ray deviation and eliminating the need for recalibrations of other parts of the optical system. The prisms are manufactured using an N-BK7 substrate and feature a high precision 40-20 surface quality, λ/8 surface flatness, and +0/-0.1mm dimensional tolerance.
Eight standard VIS 0 and NIR 1 coatings available
Coating options for the TECHSPEC® BBAR Coated Hypotenuse Right Angle Prisms include VIS and NIR coatings, which reduce surface reflections in their designated wavelength ranges for increased total transmission. Eight standard VIS 0 and NIR 1 coated prisms are available with hypotenuse lengths of 14.1mm to 70.7mm and legs from 10mm to 50mm. Custom sizes are also available. TECHSPEC® BBAR Coated Hypotenuse Right Angle Prisms are in-stock and available for immediate delivery.
About Edmund Optics:
Edmund Optics® is a leading supplier of optics, imaging, and photonics technology for the Life Sciences, Biomedical, Semiconductor, R&D, and Defense markets around the globe. Edmund Optics designs and manufactures a wide array of multi-element lenses, lens coatings, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of both stock and custom products. Edmund Optics’ state-of-the-art manufacturing capabilities, combined with its global distribution network, has earned it the position of the world’s largest supplier of off-the-shelf optical components. Customers can purchase items by calling 1-800-363-1992, via the catalog or the website at www.edmundoptics.com.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
Privacy Policy | Cookie Policy | Terms & Conditions | Accessibility
California Consumer Privacy Act (CCPA): Do Not Sell My Information
The FUTURE Depends On Optics®