eo_logo
 
Product added to cart

What are some advantages of using one plate beamsplitter type compared to another?

A plate beamsplitter is the most common type of beamsplitter. It features a thin glass substrate. The reflective coating is typically optimized at 45°, and an anti-reflection coating is commonly applied to the rear surface. Similar to cube beamsplitters, plate beamplitters also come in polarizing and non-polarizing types. Polarizing plate beamplitters split the input beam into two orthogonal components; P-polarized light is transmitted while S-polarized light is reflected 90° to it. Non-polarizing plate beamsplitters split the input beam into two orthogonal components; average, P-polarized and S-polarized states are transmitted and reflected equally. Dichroic plate beamsplitters reflect one portion of the spectrum while transmitting the other. They are ideal for splitting or combining specific wavelengths of light, depending upon the application setup. Polka-dot plate beamsplitters offer specific reflection/ transmission ratios. They have a constant reflection-to-transmission ratio over a large spectral range, making them ideal for use from UV to mid-IR. They are also not angle sensitive so they are great for splitting energy from a radiant light source. Pellicle beamsplitters offer specific reflection/ transmission ratios as well. Due to their ultra-thin nitrocellulose membrane construction, there are no ghost images from second surface reflections, no chromatic aberration with converging beams, and no change in optical path length. Elliptical plate beamsplitters maximize beamsplitter efficiency while maintaining required mounting space. When oriented at 45° they create a circular aperture equal to the diameter of the minor axis.

PolarizingNon-PolarizingLateral Displacement
Polarizing Plate Beamsplitter Non-Polarizing Plate Beamsplitter Lateral Displacement Plate Beamsplitter
這項內容對您是否實用?
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin
;