Edmund Optics 使用 cookies 来优化和增强我们网站的功能和内容。点击"确定 "以获得完整的用户体验,点击 "详细信息 "按钮可查看有关我们使用的 cookie 的其他信息。我们不会出售从营销 cookie 中获得的有关您的信息,我们仅将其用于改善您在Edmund Optics 的体验。
该提供商收集的部分数据用于个性化和衡量广告效果。
该提供商收集的部分数据用于个性化和衡量广告效果。
Through the photovoltaic effect, detectors provide a means of transforming light energy to an electrical current. The root of the theory behind this phenomenon is a small energy gap between the valence and conduction bands of the detector. When light, with enough energy to excite an electron from the valence to the conduction band, is incident upon the detector, the resulting accumulation of charge leads to a flow of current in an external circuit. Since light is not the only source of energy that can excite an electron, detectors will have some amount of current that is not representative of incident light. For example, fluctuations in thermal energy can easily be mistaken for light intensity changes. A variety of these “non-light” contributions are present and, when summed up, make up the total noise within the detector.
Type | Note | Active Area (mm2) | Package | 比較 | 庫存號碼 | 價格 | Buy | |
---|---|---|---|---|---|---|---|---|
Biased | Normal Response | 0.20 | TO-18 | #57-506 | NT$1,348 Qty 5+ NT$1,199 Request Quote |
|
||
Biased | Normal Response | 0.81 | TO-18 | #57-507 | NT$1,348 Qty 5+ NT$1,199 Request Quote |
|
||
Biased | Normal Response | 3.2 | TO-18 | #53-372 | NT$1,348 Qty 5+ NT$1,164 Request Quote |
|
||
Biased | Normal Response | 5.1 | TO-5 | #53-371 | NT$1,741 Qty 5+ NT$1,505 Request Quote |
|
||
Biased | Normal Response | 16.4 | TO-8 | #54-034 | NT$1,960 Qty 5+ NT$1,706 Request Quote |
|
||
Biased | Normal Response | 44.0 | TO-8 | #54-035 | NT$2,695 Qty 5+ NT$2,363 Request Quote |
|
||
Biased | Normal Response | 100.0 | BNC | #53-373 | NT$5,005 Qty 5+ NT$4,445 Request Quote |
|
||
Biased | Normal Response | 613.0 | BNC | #53-374 | NT$16,695 Qty 5+ NT$14,840 Request Quote |
|
||
Unbiased | Blue Enhanced Response | 0.81 | TO-18 | #57-508 | NT$1,741 Qty 5+ NT$1,505 Request Quote |
|
||
Unbiased | Blue Enhanced Response | 5.1 | TO-5 | #53-378 | NT$1,741 Qty 5+ NT$1,505 Request Quote |
|
||
Unbiased | Blue Enhanced Response | 100.0 | BNC | #53-379 | NT$4,900 Qty 5+ NT$4,375 Request Quote |
|
||
Unbiased | UV Enhanced Response | 15.0 | TO-5 | #57-510 | NT$2,695 Qty 5+ NT$2,363 Request Quote |
|
||
Unbiased | UV Enhanced Response | 20.0 | TO-8 | #54-036 | NT$2,695 Qty 5+ NT$2,363 Request Quote |
|
||
Unbiased | UV Enhanced Response | 35.0 | TO-8 | #54-037 | NT$3,745 Qty 5+ NT$3,325 Request Quote |
|
||
Unbiased | UV Enhanced Response | 50.0 | BNC | #53-376 | NT$6,090 Qty 5+ NT$5,390 Request Quote |
|
||
Unbiased | UV Enhanced Response | 100.0 | BNC | #53-377 | NT$7,245 Qty 5+ NT$6,440 Request Quote |
|
The ratio of the overall signal output to the noise level is known as the signal to noise ratio (s/n) and can be used to determine if noise will be a concern within a particular application. While noise is certainly a key means of characterizing detectors, it is only one of the characteristics which should be considered when selecting a detector.
Photovoltaic (Unbiased): During PV operation, no external bias is applied to the photodiode. Since Dark Current is a function of bias magnitude, PV operation eliminates Dark Current as a source of noise. In this case, the NEP will be lower, thereby allowing greater sensitivity at lower wavelengths. This makes it ideal for low signal detection. One disadvantage is the slightly lower responsivity at higher wavelengths (see graph).
Photoconductive (Biased): During PC operation, a reverse bias on the photodiode results in a number of response advantages, such as a faster rise time. This makes this type of operation more suitable for high frequency applications. One inconvenience is that the dark current increases with this applied biased current, so noise is introduced into the system.